News Releases
FOR IMMEDIATE RELEASE No. 3597
3.3kV SBD-embedded SiC-MOSFET module
TOKYO, May 8, 2023 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping samples of a new Schottky barrier diode (SBD)-embedded silicon carbide (SiC) metal-oxide-semiconductor field-effect transistor (MOSFET) module, featuring dual-type 3.3kV withstand voltage and 6.0kVrms dielectric strength, on May 31. The new module is expected to support superior power, efficiency and reliability in inverter systems for large industrial equipment such as railways and electric power systems. It will be exhibited at major trade shows, including Power Conversion Intelligent Motion (PCIM) Europe 2023 in Nuremberg, Germany from May 9 to 11.
Mitsubishi Electric has already released four full-SiC modules and two 3.3kV high-voltage dual-type LV100 modules. To further contribute to high power output, efficiency and reliability in inverters for large industrial equipment, the company will soon begin providing samples of its new module, which reduces switching loss as an SiC-MOSFET with a built-in SBD and an optimized package structure.
Note that the press releases are accurate at the time of publication but may be subject to change without notice.